Skip to main content
uc2013135191
Associate III
July 19, 2015
Question

SPL for F0xx, V1.5.0 .chm help file has missing info (19/Jul/2015)

  • July 19, 2015
  • 1 reply
  • 622 views
Posted on July 19, 2015 at 02:10

Just wanted to give a heads up to this.

First of all, I am sorry if it was already referenced but I could not find anything when using the search tool.

I have the V1.5.0 standard peripheral library package for F0 series. I also have V1.4.0.

One thing I noticed is that the V1.5.0 is missing all the drivers info!

There's nothing there as far as I am aware, when I got to ''Modules'' there is nothing there for them, when I searched for it further I had no success in finding the information. 

I downloaded again the package and as of now, July the 19th of 2015, the problem still persists.

To note that in V1.4.0 there was also a problem with it, the info for the timer drivers was not present in the correct place, and was instead on the page before it, named ''STM32F0xx_StdPeriph_Driver''.

I find that help file really useful and wanted to bring attention to this problem with hope it is fixed. I know most of that info can be found in the source files btw.

#.chm-f0-spl-library-help-file
    This topic has been closed for replies.

    1 reply

    Nesrine M_O
    Associate
    July 22, 2015
    Posted on July 22, 2015 at 12:16

    Hi,

    You are right;all the drivers info is missing.

    It is noted and will be fixed in coming release of the STM32F0 standard peripheral library.

    -Syrine