SPI communication with STM32H7(Master) to STM32F1(slave) with interrupt mode
Hi,
i am trying to implement a SPI communication with STM32H7(Master) to STM32F1(slave) with interrupt mode. In Slave Side SPI3(with NSS Hardware Input) i have enabled, In Master Side SPI6 (GPIO Pin Toggling for SS) I have Enabled
My Issue is at Slave Side I have this Function to receive from master HAL_SPI_Receive_IT(&hspi3, RX_Buffer, 4); and Its not Entering into -> void SPI3_IRQHandler(void) function. How we can resolve this issue? and Only one time below condition gets satisfied in HAL_SPI_Receive_IT function
"if (hspi->State != HAL_SPI_STATE_READY)"