Question
serial connection to stm32f429i discovery board
Posted on October 15, 2016 at 11:20
Hi,
I'm trying to run uclinux on my discovery board.I loaded EMcafts uboot on my board,and then I wanted to enter command mode but it is impossible!I tryed hyper terminal and tera term on windows and of course Ckermit on linux, I get this from different consoles but I cant send anything to the board and so I can NOT stop autoboot!I've been working on it for about 5 days and it makes me crazy,please help me about it!should I make some changes on my board (like removing sb11 & sb15) ? or this problem is related to software?or this is problem related to my keyboard?Guys HEEELLLPPPU-Boot 2010.03-cortexm-1.14.2 (Sep 04 2015 - 19:58:13)CPU : STM32F4 (Cortex-M4)Freqs: SYSCLK=180MHz,HCLK=180MHz,PCLK1=45MHz,PCLK2=90MHzBoard: STM32F429-DISCOVERY Rev 1.ADRAM: 8 MB*** Warning - bad CRC, using default environmentIn: serialOut: serialErr: serialNet: STM32_MACHit any key to stop autoboot: 0Wrong Image Format for bootm commandERROR: can't get kernel image!STM32F429-DISCO>