NSS input not take into account on SPI SLAVE
I have a system with 1 STM32F407 and 3 STM32F401. The 407 is the master of a communication with SPI with the 3 slaves. On the slave a use SPI in slave mode with DMA in RX/TX. On the slaves the input NSS is used in hardware mode. I have of course three GPIO on master which allow to select one slave after each other. When I try to ask a slave I receive it answer BUT all the three slave answer at the same time. It's like the slave do not take into account the NSS pin.
I have configured the system with STMCube.
I use the HAL library.
/* SPI2 init function */
void MX_SPI2_Init_STEPPER(void){hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_SLAVE; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_8BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_HARD_INPUT; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLED; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED; hspi2.Init.CRCPolynomial = 10; HAL_SPI_Init(&hspi2);}
void MX_DMA_Init_STEPPER(void)
{ /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE();/* DMA interrupt init */
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn); HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);}
HAL_SPI_TransmitReceive_DMA(&SPI_HMI,(uint8_t *)&txAxisBuffer[0],(uint8_t *)&rxAxisBuffer[0],20);
Has someone a solution for me?
Thank you in advance.
#dma-spi-slave-nss-hardware