Skip to main content
Tinnagit
Senior II
May 5, 2023
Solved

my RTC don't run after power off and RTC_BKP_DR0 was cleared

I have Nucleo G0B1RE.

I had add 3V battery to VBAT.

I had change to use LSE for RTC.

I had add RTC_BKP_DR to keep time before reset so RTC time reg was not cleared after reset but It was re-initial while booting.

But RTC don't count while power off and RTC_BKP_DR was cleared after reset.

So I don't know what my mistake?

This is my system clock config

void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
 
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
 RCC_OscInitStruct.PLL.PLLN = 8;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enables the Clock Security System
 */
 HAL_RCC_EnableLSECSS();
}

and This is my RTC Initial

static void MX_RTC_Init(void)
{
 
 /* USER CODE BEGIN RTC_Init 0 */
 
 /* USER CODE END RTC_Init 0 */
 
 RTC_TimeTypeDef sTime = {0};
 RTC_DateTypeDef sDate = {0};
 
 /* USER CODE BEGIN RTC_Init 1 */
 rtc_state = 0x01;
 /* USER CODE END RTC_Init 1 */
 
 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN Check_RTC_BKUP */
 rtc_state |= 0x02;
 if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
	 rtc_state |= 0x04;
 /* USER CODE END Check_RTC_BKUP */
 
 /** Initialize RTC and set the Time and Date
 */
 sTime.Hours = 0x0;
 sTime.Minutes = 0x0;
 sTime.Seconds = 0x0;
 sTime.SubSeconds = 0x0;
 sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sTime.StoreOperation = RTC_STOREOPERATION_SET;
 if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 sDate.WeekDay = RTC_WEEKDAY_MONDAY;
 sDate.Month = RTC_MONTH_JANUARY;
 sDate.Date = 0x1;
 sDate.Year = 0x0;
 
 if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN RTC_Init 2 */
 rtc_state |= 0x08;
 HAL_PWR_EnableBkUpAccess();
 HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
 HAL_PWR_DisableBkUpAccess();
 rtc_state |= 0x10;
 }
 /* USER CODE BEGIN RTC_Init 2 */
 
 /* USER CODE END RTC_Init 2 */
 
}

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
May 6, 2023

Did you disconnect SB26?

JW

6 replies

waclawek.jan
waclawek.janBest answer
Super User
May 6, 2023

Did you disconnect SB26?

JW

Tinnagit
TinnagitAuthor
Senior II
May 6, 2023

No I don't.

Do I need to disconnect it?

waclawek.jan
Super User
May 7, 2023

Note, that by setting BYPHSAD=1 you have to follow the "read twice, compare, repeat if no match" procedure, read the relevant chapter in RM and perhaps the second part of this.

Also, RSF after setting BYPSHAD=1 won't get set, the Cube/HAL function you're using for waiting for RSF (HAL_RTC_WaitForSynchro()) has a timeout though so that's why it won't loop forever for you. OTOH, HAL_RTC_WaitForSynchro() starts with clearing RSF without disabling the RTC registers protection, so it won't clear RSF if it was set previously, and that's another mechanism how HAL_RTC_WaitForSynchro() will appear to working just OK for you.

JW

Tinnagit
TinnagitAuthor
Senior II
May 7, 2023

Oh Thank You so much.

I had rewrite RTC initial already.

As you comment that BYPHSAD for access a shadow register is not necessary.

I just let is sync data between shadow register and actual register by HAL_RTC_WaitForSynchro

and waiting for it complete the process. that's all.

So I don't use HAL_RTCEx_EnableBypassShadow now.

Thank You so much.