Max Output drive current of Analogue Peripherals when VDD <> VDDA
Hi. I'm designing a battery powered device that use 1.8V for the MCU core and 3V for VDDA to drive the opamps and comparators.
I would like to use the output of an opamp / comparator to power a small sensor at 3V- enabling me to switch it on/off via firmware without adding additional components. It is not clear in the data sheet what the maximum I_DDA current is that can be supplied by the opamp / comparator output.
Any advise would be appreciated.
Thanks