Skip to main content
MSale.1
Senior
November 12, 2020
Question

Is there any instructions from STM on how to implement CMD53 in the SDIO interface for STM32H747?

  • November 12, 2020
  • 0 replies
  • 572 views

I try to interface Cypress 4343W Wi-Fi module with STM32H747. i managed to port WICED SDK in STM32Cube IDE but when i start to send data using CMD53 i have problems that the DPSM always active which means from my understanding that the transmission still in progress because data end flag never set. and i got wrong response from the WI-FI module.

This topic has been closed for replies.