Skip to main content
LMI2
Senior III
June 25, 2019
Question

Is there a dual core Discovery board (already)

  • June 25, 2019
  • 4 replies
  • 1060 views

I would like to play with a dual core STM32F

    This topic has been closed for replies.

    4 replies

    Uwe Bonnes
    Chief
    June 25, 2019

    There is a H745 Disco available. I do not know of a STM32F dual core.

    LMI2
    LMI2Author
    Senior III
    June 25, 2019

    Aha, STM32F != STM32H. I meant any multicore Discovery boards.

    Piranha
    Principal III
    June 25, 2019

    So You know that there are no STM32Fxxx dual core MCU, but are asking for "dual core board"? :)

    Tesla DeLorean
    Guru
    June 25, 2019
    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    LMI2
    LMI2Author
    Senior III
    June 25, 2019

    Thanks. Digikey does not list it yet. I'll have to wait a little bit more, I think. Ànd If I understood your post you linked correctly it is also a little immature.

    I was asking any multicore board, no matter what's it's name or number of cores(as long it is more than one).

    Tesla DeLorean
    Guru
    June 25, 2019

    Well support is going to be a heavy lift.

    The H747I-DISCO I have was built almost a year ago. The V-step silicon is now available and offering 480MHz M7, 240MHz M4

    The NUCLEO-H743ZI2 is now available using the V-step silicon, and I expect the H745XI version to be available very soon. This board has the ST-LINK/V3

    https://community.st.com/s/question/0D50X0000AyCT8KSQW/new-nucleoh743zi2-out

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..