Is the backup domain operates directly out of Vdd or Vbat ?
Microcontroller used : STM32F779NI
Question:
[1] My understanding is that the backup domain is directly supplied from Vdd or Vbat (When Vdd is removed) without any regulation (1.8V to 3.6V).
Does this means below blocks can operate directly using Vdd or Vbat ?
[1] RTC
[2] RTC backup registers
[3] LSE oscillator
[2] Regarding backup SRAM, when Vdd is the supply, backup SRAM is directly powered from Vdd without any further regulation. Am i right ?
[2] Regarding backup SRAM, when Vbat is the supply, backup SRAM is powered through the low-power regulator which steps downs Vbat to 1.2 V. LP regulator is just required only during Vbat supply. Am i right ?
Regards,
Vinoth