Skip to main content
JongOk Baek
Associate III
March 17, 2017
Question

I want to get information for STM32H7 Series.

  • March 17, 2017
  • 3 replies
  • 1989 views
Posted on March 17, 2017 at 02:14

Hello.

I want to know more specification of STM32H7 series.

But, Information was not in ST site.

So I want to get datasheet and reference manual for STM32H7.

If it is possible to share, could you open more information.

I am waiting...

    This topic has been closed for replies.

    3 replies

    Nesrine M_O
    Associate
    March 17, 2017
    Posted on March 17, 2017 at 11:30

    Hi

    Baek.JongOk

    ,

    We are glad to see

    your interest on the new STM3H7series.

    As said during the announcement, the STM32H7 variants will become available along Q2-2

    https://community.st.com/0D50X00009XkihHSAR

    -Nesrine-

    Uwe Bonnes
    Chief
    March 17, 2017
    Posted on March 17, 2017 at 12:00

    Glimpses of information get available, as STM contributes to the Linux kernel:

    - [PATCH 0/5] Add STM32 DMAMUX support

    -

    https://lkml.org/lkml/2017/3/15/143

    Why is general release of chip coupled to release of reference manual?

    AvaTar
    Senior III
    March 17, 2017
    Posted on March 17, 2017 at 12:20

    Why is general release of chip coupled to release of reference manual?

    My guess - to keep the Errata documents short ... ;)

    Vladislav Datciy
    Explorer
    April 25, 2017
    Posted on April 25, 2017 at 20:31

    Is there any information about the release dates in lqfp208 package?)

    AvaTar
    Senior III
    July 10, 2017
    Posted on July 10, 2017 at 08:38

    The Keremi newsletter (www<dot>keremi<dot>com) from last states:

    STMicroelectronics removed the STM32H753 in the higher temperature grade from the site.

    Seems there is still ongoing development and validation ...

    STOne-32
    Technical Moderator
    July 16, 2017
    Posted on July 16, 2017 at 16:57

    Dears,

    You can check our web site and this new family is at evaluation phase and at production for OEM and few customers, so not yet in full production for all mass market customers. Full validation and qualification of new Technology Flash node of our STM32 MCUs is very important for us and for our customers  {You  ;) }  as we did in the past to all previous series : 180nm, then 130nm/110nm, then 90nm ( STM32F2/F4/F7 and STM32L4)  and now 40nm  with STM32H7xx. 

    Stay Tuned with us, you will release information on our web site, when we are ready !

    Cheers,

    STOne-32.