I am new and I need some help programming a PWM on the micro STM32F303ZET6
- November 15, 2021
- 5 replies
- 4559 views
I am programming a output PWM using the timers on this processor. since I am new, I decided to start using the examples for this specific processor found in the folder 'en.stm32cubef3_v1.11.0'
As a first instance I execute the project file in the folder I attached here 'SW4STM32". I place that folder into my workspace . when I execute this file the software pretty much set everything form me. but when I build the project always an error shows up:
22:12:56 **** Incremental Build of configuration Release for project STM32F303ZE-Nucleo ****
make all
make: *** No rule to make target 'C:/Users/steph/OneDrive/Documentos/Src/stm32f3xx_hal_msp.c', needed by 'Example/User/stm32f3xx_hal_msp.o'. Stop.
"make all" terminated with exit code 2. Build might be incomplete.
22:12:57 Build Failed. 1 errors, 0 warnings. (took 250ms)
The other way I am trying to do my project is creating a new 'SM32 project', once I select the processor I have and select C++ as the language. the software set everything for me and create a template of the main.c/main.h file which I replace with the files attached here. In this case the error I am sure is because there is a file missing in the folder, the file is "stm32f3xx_nucleo_144.h". This file contains some variable declarations as "TIM_HandleTypeDef TimHandle;"
Could you please help me out with this. I am a little confuse regarding this