Skip to main content
mrxx99
Visitor II
July 5, 2016
Question

How to use both Display layers on STM32F469NI?

  • July 5, 2016
  • 0 replies
  • 475 views
Posted on July 05, 2016 at 18:59

Hello,

I have the following problem: I want to use the background layer to display a background and the foreground layer to place lines above it, so that I can delete the lines without doing anything to the background. There are the function BSP_LCD_LayerDefaultInit(LayerIndex, FB_Address) and  BSP_LCD_SelectLayer(LayerIndex) but if I select the second layer nothing can be displayed. I am using the Address 0xC0000000 and Index 0 for the background layer (wdoes works) and Address 0xC0400000 and Index 1 for the foreground layer (does not work). The Addresses are taken from a datasheet of this board.

I don't know if I am doing something wrong of if this a bug like that one with the portrait mode.

Note: I am programming over mbed.org

I would be glad if anyone could help me.

#stm32f469-discovery #stm32f469
This topic has been closed for replies.