How to enable 3 multi-ranging sensors by polling mode on x-NUCLEO-53L1A1???
Description:
We currently implement 3 multi-ranging sensors on x-NUCLEO-53L1A1 by polling mode,
implementing in AutonomousLowPowerRangingTest(),There are some problems found that when I try to change sensor I2C device address to
left = 0x54, center = 0x56, right = 0x58. SW will get error return code as -15 (VL53L1_ERROR_DIVISION_BY_ZERO).but if I try to enable ONLY ONE sensor by addr = 0x52 (default), it can be working without problem.
So my question is, do 3 sensors share same I2C as 0x52 and if so, how to get each sensor values?I attach my code for reference
== start
void AutonomousLowPowerRangingTest(void)
{ static VL53L1_RangingMeasurementData_t RangingData; uint8_t byteData; printf('Autonomous Ranging Test\n');status = XNUCLEO53L1A1_ResetId(1, 0); // Reset ToF sensor
HAL_Delay(2); status = XNUCLEO53L1A1_ResetId(1, 1); // Reset ToF sensor HAL_Delay(2);//status = VL53L1_SetDeviceAddress(Dev, 0x56);
//HAL_Delay(2);status = VL53L1_WaitDeviceBooted(Dev);
HAL_Delay(2);Dev->I2cDevAddr = 0x56;
status = VL53L1_DataInit(Dev); -> IT FAILS here by -15 status = VL53L1_StaticInit(Dev); status = VL53L1_SetDistanceMode(Dev, VL53L1_DISTANCEMODE_LONG); status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(Dev, 50000); status = VL53L1_SetInterMeasurementPeriodMilliSeconds(Dev, 500); status = VL53L1_StartMeasurement(Dev); status = XNUCLEO53L1A1_ResetId(0, 1); // Reset ToF sensor HAL_Delay(2); status = VL53L1_WaitDeviceBooted(DevL); status = VL53L1_SetDeviceAddress(DevL, 0x54); HAL_Delay(2); Dev->I2cDevAddr = 0x54;status = VL53L1_DataInit(DevL);
-> IT FAILS here by -15
status = VL53L1_StaticInit(DevL); status = VL53L1_SetDistanceMode(DevL, VL53L1_DISTANCEMODE_LONG); status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(DevL, 50000); status = VL53L1_SetInterMeasurementPeriodMilliSeconds(DevL, 500); status = VL53L1_StartMeasurement(DevL);status = XNUCLEO53L1A1_ResetId(2, 1); // Reset ToF sensor
HAL_Delay(2); status = VL53L1_WaitDeviceBooted(DevR); status = VL53L1_SetDeviceAddress(DevR, 0x58); HAL_Delay(2); Dev->I2cDevAddr = 0x58;status = VL53L1_DataInit(DevR);
-> IT FAILS here by -15
status = VL53L1_StaticInit(DevR); status = VL53L1_SetDistanceMode(DevR, VL53L1_DISTANCEMODE_LONG); status = VL53L1_SetMeasurementTimingBudgetMicroSeconds(DevR, 50000); status = VL53L1_SetInterMeasurementPeriodMilliSeconds(DevR, 500); status = VL53L1_StartMeasurement(DevR);== end