How to detect falling/rising edge or high/low pulse in STM32F405
Hello
I am working on STM32F405. I need to detect falling/rising edge or high/low pulse using timer capture mode. Basically I am trying to interface an IR remote which works on RC5 protocol with STM32. But before that I just want to know how to detect high/low pulses. For this, I am using Timer8 Channel 3 which is on PC8. I have a connected gpio to this PC8 and toggling this GPIO with 500ms. I want to capture this pulse with 500ms high and 500ms low. Below is the code I am using :
/***** GPIO PIN *******/
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
GPIO_InitTypeDef GPIO; GPIO.GPIO_Pin = GPIO_Pin_10; GPIO.GPIO_Speed = GPIO_Speed_100MHz; GPIO.GPIO_Mode = GPIO_Mode_OUT; GPIO.GPIO_OType = GPIO_OType_PP; GPIO.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD,&GPIO);GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE);RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_TIM8); NVIC_InitStructure.NVIC_IRQChannel = TIM8_CC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); TIM_ICInitTypeDef TIM_ICInitStructure;TIM_ICInitStructure.TIM_Channel = TIM_Channel_3; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0;TIM_ICInit(TIM8, &TIM_ICInitStructure);
TIM_Cmd(TIM8, ENABLE);TIM_ITConfig(TIM8, TIM_IT_CC2, ENABLE);
I have put the GPIO toggling code inside while(1) with the delay of 500ms.
Below is the interrupt
void TIM8_CC_IRQHandler(void)
{
if(TIM_GetITStatus(TIM8, TIM_IT_CC2) == SET)
{
//it enters in this if condition but failed to capture
int temp = TIM_GetCapture2(TIM8); //value of temp remains 0
}
}
What is wrong in the code.? Please help.
#timer #stm32-f #input-capture