Skip to main content
YGaju.1
Associate II
August 11, 2022
Question

How to create new STM32 project for only 1 core for a dual core controller (STM32H757 Eval board)

  • August 11, 2022
  • 3 replies
  • 1676 views

I want to create project for only CM7 core. But, now what happens is when I try to create a new STM32 project for STM32h757 controller, then it creates 2 projects CM7 & CM4 inside 1 project.

I have tried by deleting CM4 project, then built CM7, its building. But I find this as a workaround solution.

Need a solution for properly creating a project for single core.

This topic has been closed for replies.

3 replies

Bowman32
ST Employee
August 12, 2022

Hi @YGaju.1​ 

The two cores boot either separately or together. This is configurable using dedicated option bytes BCM7 and BCM4.

Please refer to RM0399 Rev 3, section 2.6 describes the boot configuration. Also, in AN5557, a dedicated section 3.2 Dual-core boot.

YGaju.1
YGaju.1Author
Associate II
August 16, 2022

Hi Bouraoui Chemli ,

Thanks for your reply.

Ya I understand that these 2 cores can be managed by the option byte, and later you can disable/ enable it from the option byte. But, I was trying to figure out a way to create only a project where I have only 1 core. (i.e. CM7).

For eg. if I create a new STM32 project for STM32H757 controller, then a project is created inside which 2 more nested projects are created each for CM7 and CM4. But, in my case I need project to be created for only 1 core whenever I create a new STM32 project.

Bowman32
ST Employee
August 16, 2022

Hi @YGaju.1​ 

The STM32CubeMX is in line with default templates, it generate a project for each core.

  • BootCM4_CM7
  • BootCM7_CM4Gated  
  • BootCM4_CM7Gated
  • BootCM7_CM4Gated_RAM

Templates are provided in STM32CubeH7 package via this path: STM32Cube_FW_H7_V1.10.0\Projects\STM32H747I-EVAL\Templates

Maybe you can adapt STM32H743 example to your need.