Skip to main content
Associate II
May 17, 2019
Question

How did I damage the STM32F030R8 with external power to DISCOVERY?

  • May 17, 2019
  • 3 replies
  • 1181 views

In a word: I seem to have damaged the flash on an STM32F0 Discovery board by attaching external power.

Details

I had peripherals attached to the STM32F030R8-Discovery board that required more than 100mA @ 3V available from the Discovery's on-board regulator. I attached a 3.3VDC supply to the 3V pin (pin 1) of the board and let it common ground with GND (pin2). 5V was still provided by USB.

Ever since then, I am unable to flash the STM32F0 . I've removed all my external logic. I was using the same studio and the Discovery's on-board STLINK ability, as always. My understanding of the Discovery is that diodes protect both the on-board 5V (diode drop from USB, so, more like 4.5V) and 3V supplies from external power. But I must have somehow overdriven the STM32.

I can still connect and interrogate the STM32F0. Reading flash shows a few non-FF bytes at 0x0800 0000 but then the rest of the device is blanked. I had attempted a bulk erase at one time and it must have partially completed. The loader etc. at 0x1FFF EC00 is not erased. The option bytes are all 0xFF'd - fortunately that's the default and flash is not write-protected..

I am replacing the Discovery but will need to repeat this. Any advice for how to avoid damaging a second Discovery?

The log of a download to flash from stutil that fails is as follows:

  1. 2019-05-17T11:06:50 INFO src/common.c: Loading device parameters....
  2. 2019-05-17T11:06:50 INFO src/common.c: Device connected is: F0 device, id 0x20006440
  3. 2019-05-17T11:06:50 INFO src/common.c: SRAM size: 0x2000 bytes (8 KiB), Flash: 0x10000 bytes (64 KiB) in pages of 1024 bytes
  4. 2019-05-17T11:06:50 INFO src/gdbserver/gdb-server.c: Chip ID is 00000440, Core ID is 0bb11477.
  5. 2019-05-17T11:06:50 INFO src/gdbserver/gdb-server.c: Listening at *:4500...
  6. 2019-05-17T11:07:06 INFO src/gdbserver/gdb-server.c: Found 4 hw breakpoint registers
  7. 2019-05-17T11:07:06 INFO src/gdbserver/gdb-server.c: GDB connected.
  8. 2019-05-17T11:07:15 INFO src/common.c: Attempting to write 1024 (0x400) bytes to stm32 address: 134217728 (0x8000000)
  9. Flash page at addr: 0x08000000 erased
  10. 2019-05-17T11:07:15 INFO src/common.c: Finished erasing 1 pages of 1024 (0x400) bytes
  11. 2019-05-17T11:07:15 INFO src/common.c: Starting Flash write for VL/F0/F3/F1_XL core id
  12. 2019-05-17T11:07:15 INFO src/flash_loader.c: Successfully loaded flash loader in sram
  13. 2019-05-17T11:07:18 ERROR src/flash_loader.c: flash loader run error
  14. 2019-05-17T11:07:18 ERROR src/common.c: stlink_flash_loader_run(0x8000000) failed! == -1

This topic has been closed for replies.

3 replies

spectatorAuthor
Associate II
May 17, 2019

Well, I had a USB serial translator chip attached to USART1 when this all started, and perhaps somehow it was preventing bootloader activation. No other idea.

But after I was having trouble flashing the STM32F0, my clumsy erases evidently did 0xFF-erase the option bytes. I suspect that changing nBOOT1 to 1 is preventing the serial bootloader on the STM32F030R8 from activating. Unless there is still some other way to revert the option nBOOT1 to 0, I am afraid I have bricked the STM32F0.

Mon2
Senior III
May 18, 2019

Have not lived through your experience but...if you had voltages being applied onto the I/O pins of the CPU but the CPU was not being powered then it is possible that you faced a reverse voltage feed (bias) and caused these events. Summary, the CPU must be powered before you apply external voltages onto the I/O pins of the device. Ok to have the CPU powered up first but best if both powered up at the same time.

spectatorAuthor
Associate II
May 18, 2019

Thank you for your reply. At one point, I did put all the external components on their own supply/domain and gated that power domain with a GPIO-controlled nFET. I saw some back powering along the SPI channel for a moment (forgot a pull-down on the gate), and this would have been the problem you described. I will have to be more careful while prototyping this on the replacement Discovery.