Question
Hi all, because just I have jumped to ST32 MCU, I would like ask you for help with follow general answer if its possible to do with this MCU. I have chosen MCU STM32G031G4.
I need to generate:
- 7 independent PWM channels, I/O outputs
- each channel will have 3 dependent PWM signals with phase shift 120 degrees ( total I/O outputs is 21 PWM channels)
- Frequency for all channels should be 3MHz
- Duty cycle of all PWM should vary from 1 to 99 % and has to be control by analog value by ADC
- Duty cycle has to change for each PWM channel from basic value to requested value in 0.5us
Do you think that core of this MCU is able fulfill these tasks? Is necessary to choose another one or not.
Thank you very much.
Best Regards,
Miro