Skip to main content
AElah.1
Visitor II
December 25, 2022
Question

Do I have to use STM32 HAL for Keil uvision Run Time Environment ( Device start up File

  • December 25, 2022
  • 1 reply
  • 770 views

I am Using STM32L152 with Keil uvision5 and for setup Run Time Environment must selct STM32cube HAL library, do I have to use HAL or I can use only device start up

This topic has been closed for replies.

1 reply

Technical Moderator
January 27, 2023

Hello @AElah.1​,

Indeed, it is possible to use device's startup file. However, It is recommended to use HAL for ease of use and functionalities.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL