DMA transfers 25% of buffer in memory to memory mode
Using STM32F417 DMA and got it to work but it only transfers 25% of the buffer size indicated. So far, I have tested the following buffer sizes:
Buffer size (bytes) Bytes transferred
10 3
25 7
1000 250
So, that's 25% ceiling to the next higher integer. If there is some other math relationship, please let me know.
Here is my code for the DMA, followed by the interrupt handler:
#define DMA_STREAM DMA2_Stream0
#define DMA_CHANNEL DMA_Channel_0
#define DMA_STREAM_CLOCK RCC_AHB1Periph_DMA2
#define DMA_STREAM_IRQ DMA2_Stream0_IRQn
#define DMA_IT_TCIF DMA_IT_TCIF0
#define DMA_STREAM_IRQHANDLER DMA2_Stream0_IRQHandler
void InitDMAmemory( void ) //////////////////////////////////////////////////
{
DMA_InitTypeDef dma_mem;
NVIC_InitTypeDef NVIC_InitStructure;
uint32_t Timeout = TIMEOUT_MAX;
// Start the DMA clock
RCC_AHB1PeriphClockCmd(DMA_STREAM_CLOCK, ENABLE);
// DeInit to reset DMA config to default reset value
DMA_DeInit(DMA_STREAM);
while(DMA_GetCmdStatus(DMA_STREAM) != DISABLE)
{
}
// Set values for parameters
dma_mem.DMA_Channel = DMA_CHANNEL;
dma_mem.DMA_Memory0BaseAddr = (uint32_t)memBuffer;
dma_mem.DMA_PeripheralBaseAddr = (uint32_t)periphBuffer;
dma_mem.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;
dma_mem.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
dma_mem.DMA_DIR = DMA_DIR_MemoryToMemory;
dma_mem.DMA_Mode = DMA_Mode_Normal;
dma_mem.DMA_MemoryInc = DMA_MemoryInc_Enable;
dma_mem.DMA_PeripheralInc = DMA_PeripheralInc_Enable;
dma_mem.DMA_BufferSize = BUFFERSIZE;
dma_mem.DMA_Priority = DMA_Priority_High;
dma_mem.DMA_MemoryBurst = DMA_MemoryBurst_Single;
dma_mem.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
dma_mem.DMA_FIFOMode = DMA_FIFOMode_Enable;
dma_mem.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_Init(DMA_STREAM, &dma_mem);
DMA_ITConfig(DMA_STREAM,DMA_IT_TC, ENABLE);
while ((DMA_GetCmdStatus(DMA_STREAM) != ENABLE) && (Timeout-- > 0))
{
}
/* Check if a timeout condition occurred */
if (Timeout == 0)
{
/* Manage the error: to simplify the code enter an infinite loop */
while (1)
{
}
}
/*Enable DMA1 Stream IRQ Channel */
NVIC_InitStructure.NVIC_IRQChannel = DMA_STREAM_IRQ;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
DMA_Cmd(DMA_STREAM, ENABLE);
} // end InitDMAmemory ///////////////////////////////////////////////////////////
void DMA_STREAM_IRQHANDLER( void ) //////////////////////////////////////////////
{ //Test on DMA1 Channel1 Transfer Complete interrupt if(DMA_GetITStatus(DMA_STREAM, DMA_IT_TCIF)) { status=1; DMA_ClearITPendingBit(DMA_STREAM,DMA_IT_TCIF); DMA_Cmd(DMA_STREAM,DISABLE); DMA_ITConfig(DMA_STREAM, DMA_IT_TC, DISABLE); } } // end DMA1_Stream3_IRQHandler //////////////////////////////////////////////////I can't figure out why the whole transfer is not being completed. Is the transfer complete interrupt occurring early? Why does do a percentage instead of a discrete number?
Thank you for your help!