Crystal Oscillator for STM32F407 connected to LAN8720
I'm planning to build a custom board with STM32F407 chip for a system where I also need Ethernet connectivity.
I'm planning to connect this board to a LAN8720 with breakout board from Smart Electronics to have Ethernet connectivity (two independent boards connected via PHY interface).
But I'm a bit in doubt regarding which Oscillator to couple with STM32F407.
I read that for RMII we need a 25MHz oscillator to achieve the 50MHz required for RMII circuit. But I also notice that breakout board already its own 50MHz crystal oscillator.
I also notice that some of these boards do not include this extra crystal oscillator, not the case with the board I have.
In this case I still need the use a 25MHz crystal oscillator with STM32F407 or can I use the "standard" 16MHz crystal that also comes with a lot of available boards (DevEBox, DiyMoore, etc).
Thanks in advance!
Cheers,
Leandro