Skip to main content
Associate
July 4, 2023
Question

Bluepill to STM32F446 with CAN Bus

  • July 4, 2023
  • 0 replies
  • 912 views

Hi. I have developed a CAN based protocol to a Bluepill and now I need to test that on the Nucleo board as well. I have been trying this for a while now and for some reason CAN messages are generated from the Nucleo board. The code was working fine with Bluepill and I need some guidance to change the paltform to Nucleo. PS:I am pretty sure that the custom built libraries are platform independent. 

This topic has been closed for replies.