Skip to main content
BLowr.1
Associate
July 24, 2021
Question

Advanced TIM1 and TIM8 won't drive output as PWM mode as output

  • July 24, 2021
  • 2 replies
  • 1757 views

General timers work fine as PWM. Using TIM2, TIM3, TIM4 and TIM9 as well. They all work.

TIM1 and TIM8 the advanced timers will not drive output pin, no matter how I configure unit.

Using external clock 8Mhz as clock source, have tried internal clock source as well.

Output port pin is configured correctly on advanced function. Can see in debug, all registers in TIM8 are configured correctly. Can pause in debug mode and see timer increment correctly. I've Tried TIM8 Channel 1 and Channel 4. No deadtime configured as using single output of positive polarity.

I've tried to configure just TIM8 and still no output

Burke Lowrey

lowrey@live.com

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
July 24, 2021

Set TIMx_BDTR.MOE.

JW

PS. Next time, please start whit stating which STM32 are you using and post content of relevant registers.

BLowr.1
BLowr.1Author
Associate
July 24, 2021

you are my hero!!!

Is 32STMF446RCT

had tried earlier setting MOE bit in debug, and would not let me change it.

After config of no Break and Dead Time. I did the following in the code and it worked.

if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK)

 {

  Error_Handler();

 }

 htim8.Instance->BDTR |= 0x8000;

Thank you very much.

Burke Lowrey