Skip to main content
onlycoke
Visitor II
May 13, 2014
Question

About License of ''STMicroelectronics Virtual COM Port''

  • May 13, 2014
  • 2 replies
  • 689 views
Posted on May 13, 2014 at 09:21

Hi guys

Is there someone who knows License of ''STMicroelectronics Virtual COM Port''?

Now, I'm developing a device that is included USB CDC function.

It's working pretty well.

In this moment, I want to apply our company's VID & PID to this driver and USB descriptor.

I think it is not hard job.

But I worry about License of ''STMicroelectronics Virtual COM Port''.

Can i use ''STMicroelectronics Virtual COM Port'' windows driver without any license for commercial goods?

If there is something which are license and processing, Please let me know.

#license
    This topic has been closed for replies.

    2 replies

    chen
    Associate II
    May 13, 2014
    Posted on May 13, 2014 at 15:18

    '' want to apply our company's VID & PID''

    Once you change the VIP & PID - the driver that will be loaded may be different.

    It is up to the company developing the device to develop the install package ( the .inf file ).

    In any case, my understanding is the the ST VCP driver is just a wrapper for the built in Windows USB CDC default driver. The .inf file just tells Windows to use the default USB CDC device drive for the ST PID