Question
STM32H750XBH6 BGA soldering
Hi there.
I got in trouble with H750XBH6.
I designed a costum board base on mcu above.
I followed datasheet recommendations for BGA footprint.
Now I got problem with soldering. The pads are too small and doesn't make connection with chip balls.
So the chip doesn't work properly and I guess there are many of non-connected pins specially on GND and VCC pins under chip.
I got confused about the 0.225mm pad recommendation in datasheet.
Why the pads are smaller than the chip balls?
The balls are about 0.4mm