Skip to main content
FDigi
Associate III
November 13, 2019
Question

I using a board STM32l412 Nucleo 64 and I would like to use its ST-Link to load a firmware in other MCU (external application) , but the ST-Link does not connect to the other board. The hardware connection is ok.

Is there some software configuration to do this procedure?

Thanks

This topic has been closed for replies.

6 replies

Uwe Bonnes
Chief
November 13, 2019

How did you test the hardware connection if the ST-Link does not connect?

Did you try "connect under reset"

Is the target IO-Voltage 3.3 VolT? If less, Debugger will not recognize the level.

Can you test with another debugger?

Di you see signal on the connection with a scope?

FDigi
FDigiAuthor
Associate III
November 14, 2019

How did you test the hardware connection if the ST-Link does not connect?

I mean the wiring connection.

Did you try "connect under reset"

Not yet.

Is the target IO-Voltage 3.3 VolT?

Yes.

Can you test with another debugger?

I can connect with J-Link.

Di you see signal on the connection with a scope?

Not yet.

Tesla DeLorean
Guru
November 13, 2019

You have a common ground?

​

Most often it is that the design you connect too is nonfunctional.

​

Check you have VDDA connected.

Check part orientation.

Check level on NRST.

Check voltages and capacitors on VCAP pin(s)​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FDigi
FDigiAuthor
Associate III
November 14, 2019

I can connect to design with J-Link.

Mike_ST
ST Technical Moderator
November 13, 2019

If not already done, you have to remove jumpers on CN2 and JP4.

It is recommended to update the ST-Link firmware as well.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
FDigi
FDigiAuthor
Associate III
November 14, 2019

Yes, jumpers removed.