Use CubeProgrammer as UART Mode
Hey there,
i want to reach my flash memory through UART. I can do this with ST-Link device but now i want to do it with UART. I use STM32F091CC MCU and as datasheet says i configured the UART pins(PA9-PA10) as Asynchronus UART in CubeMX.
My baud rate is 9600 bits/s- word legth 8bits - parity - even and stop bit is 1.
In boot mode configuration. I try to use all configurations but i cannot reach the flash memory.
I coded all options(set and clear bitss) in main.c program and when i click connect button in cube programmer it gives me an error like that:
Please help me how to solve this problem.
Regards