Skip to main content
ABasi.2
Senior
June 29, 2025
Solved

BLE_HeartRateThreadX example file ioc not present

  • June 29, 2025
  • 2 replies
  • 612 views

Hello!

i'm trying the example BLE_HeartRateThreadX 

but the ioc file is not present in the directory, is that normal? i'm missing it?

 

also the directory arent arranged like a project maked with cube ide

is it possible to have an example that is maked like a cube ide project using the MCU or board selector?

 

thank you!

best reguards

Best answer by STTwo-32

Hello @ABasi.2 

The BLE_HeartRateThreadX and the BLE_p2pServerThreadX are not made based on the STM32CubeMX. So, there is not a ThreadX + BLE example for the STM32WB that is based on a .ioc file.

Best Regards.

STTwo-32

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
July 1, 2025

Hello @ABasi.2 

The BLE_HeartRateThreadX and the BLE_p2pServerThreadX are not made based on the STM32CubeMX. So, there is not a ThreadX + BLE example for the STM32WB that is based on a .ioc file.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ABasi.2
ABasi.2Author
Senior
July 1, 2025

Hello  STTwo-32

but why? 

there is another example that have a project created with cubeIDE for the same board? that explain the BLE communication

 

thank you!

 

best reguards 

Andrew Neil
Super User
July 2, 2025

@ABasi.2 wrote:

but why? 


Not everyone uses (or wants to use) CubeMX ?

It demonstrates that life without CubeMX is possible ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
July 1, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.