Skip to main content
asherman
Associate III
May 27, 2003
Question

ST7 BE USED FOR A RS232

  • May 27, 2003
  • 3 replies
  • 658 views
Posted on May 27, 2003 at 15:08

ST7 BE USED FOR A RS232

This topic has been closed for replies.

3 replies

asherman
ashermanAuthor
Associate III
May 22, 2003
Posted on May 22, 2003 at 10:13

Hello

CAN ST7 BE USED FOR A RS232 COMMUNICATION WHEN USING INTERNAL RC OSC. ?

IS THERE ANY APPLICATIONS FOR IT?

WE NEED BAUD RATE OF 2400.

I WOULD LIKE TO ADD THAT THE COMMUNICATION IS BETWEEN PC TO MY DEVICE.

Shermantec

itsmejatinus
Associate III
May 22, 2003
Posted on May 22, 2003 at 11:01

Yes, there is an application note available for it i.e. AN1530.This application note calliberates the SCI parameter w.r.t internal RC variation.This AN ia valid for the micros which have SCI inbuilt.

There is an another AN 973 (SCI Software Communication with a PC Using ST72251 16-Bit Timer) in case SCI peripheral is not available.

For Lite, internal RC has 1% tolerance, but SCI peripheral is not available.
stephanie
Visitor II
May 27, 2003
Posted on May 27, 2003 at 15:08

A RS232 software driver dedicated to litex is under writing and will be soon availble!