Skip to main content
JRing.2
Associate
September 13, 2021
Question

STM8S: TIM5-PWM frequency and duty cycle measure.

I am trying to measure the frequency and duty cycle of a PWM input on TIM5 channel 1. My frequency is being measured correctly but the duty cycle is not.

GPIO_Init(GPIOD, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT); //PWM input

I am using the 16MHz HSI clock with no Prescaler.

As detailed below, I am using channel 1 to capture the rising edge. I am using channel 2 to capture the falling edge from channel 1. Channel 2 triggers the interrupt.

TIM5_DeInit();

    TIM5_TimeBaseInit(3, 65000); //Prescalar = 8 (2^3)->2MHz...Count up to 65,000 before resetting counter.

    TIM5_CCxCmd(TIM5_CHANNEL_1, ENABLE);

  TIM5_CCxCmd(TIM5_CHANNEL_2, ENABLE);

TIM5_PWMIConfig(TIM5_CHANNEL_1, 

TIM5_ICPOLARITY_RISING,

TIM5_ICSELECTION_DIRECTTI, 

TIM5_ICPSC_DIV1, 

1);

TIM5_PWMIConfig(TIM5_CHANNEL_2, 

TIM5_ICPOLARITY_FALLING, 

TIM5_ICSELECTION_INDIRECTTI, 

TIM5_ICPSC_DIV1, 

1);

 

TIM5_ClearFlag(TIM5_FLAG_CC2);

TIM5_ITConfig(TIM5_IT_CC2, ENABLE);

TIM5_Cmd(ENABLE);

Interrupt Logic:

if(TIM5_GetFlagStatus(TIM5_FLAG_CC2))

 {

rise_cnt=TIM5_GetCapture1();

fall_cnt=TIM5_GetCapture2();

TIM5_ClearITPendingBit(TIM5_IT_CC2);

TIM5_ClearITPendingBit(TIM5_IT_CC1);

}

Calculations: (I do take into account the 65,000 count up roll over.)

Period_**** = rise_cnt - prev_rise_cnt

Freq=2,000,000 / Period_****

Duty_Cycle = (fall_cnt-rise_cnt)/Period_****

What am I missing?

    This topic has been closed for replies.

    4 replies

    Peter BENSCH
    ST Technical Moderator
    September 14, 2021

    Welcome, @JRing.2​, to the community!

    TIM5 does not overflow at 65000, but at 2^16 = 65536, i.e. counts from 0 ... 65535.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    JRing.2
    JRing.2Author
    Associate
    September 14, 2021

    TIM5_TimeBaseInit(3, 65000); sets my auto-reload register which causes the counter to roll over at 65000. Even if I change it to 2^16, my duty cycle capture is not functioning correctly.

    Peter BENSCH
    ST Technical Moderator
    September 14, 2021

    What does "not functioning correctly" mean exactly?

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    JRing.2
    JRing.2Author
    Associate
    September 14, 2021

    I am sending it a PWM signal 2KHz, 70% duty cycle. I confirm this with an oscilloscope. With the above settings, I measure a rising edge every 1000 counts, as I should. I should be getting a falling edge 700 counts after that. Instead, the falling edge is captured at 200.