Skip to main content
SRava.3
Visitor II
May 18, 2022
Question

I3G4250D of VDD can operate on 2.4V to 3.6V and VDDIO operate on 1.71V to VDD+0.1V, Here if we put 3.3V/3.0V on VDD and 1.8V on VDDIO then is there any limitation we can face? Core voltage(VDD) and VDDIO voltage can be different?

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    May 18, 2022

    Welcome, @SRava.3​, to the community!

    yes, this setup is possible, i.e. VDD_IO = 1.8V. But you have to connect the pull-up resistors between the I2C lines and VDD_IO. In addition, the IO voltage of the controlling microcontroller must also be at the same level, i.e. here 1.8V, either directly or via a level shifter.

    And yes, core voltage VDD and io voltage VDD_IO can be different. But in this case you should put an additionally blocking capacitor of 100nF between VDD_IO and common GND.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.