Hi @EGeor.1 ,
Well, some of these parameters are not declared in the datasheet, so I can only give an idea of typical values. For the 1.Operating temperature and 2.Storage temperature, you can refer to the datasheet, p. 14, "Absolute maximum ratings" table, last lines.
About the topics regarding the junction (point 4. to 7.), the LIS2DE12TR max supply is 3.6V and max current (normal mode, max ODR) is about 200uA, so the power consumed in the worst case is P=V*I=0.72mW. If you consider that the package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT < 0.1°C.
Moreover, no worry about the junction temperature with respect to storage temperature.
-Eleon