Skip to main content
michaelkroneberger9
Associate
December 22, 2011
Question

L6470: Output resolution, no different between 1/128 and 1/32?

  • December 22, 2011
  • 3 replies
  • 762 views
Posted on December 22, 2011 at 15:03

Hi

We have measured the output signals of the bridges in 1/128 and 1/32 step mode and we can’t see a different voltage resolution between these 2 modes (see attachment).

We have used the “GoToâ€�-command for the positioning, and mostly we can see a repositioning of the motor after the 4th step only in the 1/128-step mode (what  confirms with the measured values).

Is there any limitation of the output resolution?

Best Regards

Michael

This topic has been closed for replies.

3 replies

Enrico Poli
ST Employee
January 10, 2012
Posted on January 10, 2012 at 10:35

Dear Mike,

the voltage resolution is limited by the integrated PWM modulator of the driver (8 bit).

Using low KVAL values (in attached example you are operating below 10% of the full range), the voltage difference between two next microsteps could be below the PWM modulator limit.

Kind Regards

Enrico

michaelkroneberger9
Associate
January 24, 2012
Posted on January 24, 2012 at 07:28

Hi Encrico,

Yes, meanwhile I came to the same result; I have calculated it, and it fits to the measuring values.

Is the maximum value (255) equal to 100% KVAL or is there any additional reserve?

Regards

Michael

Enrico Poli
ST Employee
January 25, 2012
Posted on January 25, 2012 at 14:10

Hi Michael,

the maximum value of KVAL il 100% that is equivalent to a sinewave with a peak value equal to VS. There's no way to obtain higher values.

Regards

Enrico