User Activity

Processor Name: STM32MP157 Arm®-based dual Cortex®-A7 32 bits + Cortex®-M4 32 bits MPU Kernal Version: 5.10.10linux destro : openst linuxCrankstorybaord Version : 7.1OpenGLL Version : 2.0Screen Size : 1024 X 768I am developing medical GUI application...
Hi all,   I am trying to flash a custom board based on stm32mp157c based MPU. I have my own flashlayout which is also attached here.   I am constantly running into the following error.   an error occured while setting virtual partition 0xF1 alternate...
Hi all,I am trying perform build for yocto for the DK2. But running into the following error. I am pretty sure this was working until a month back but now link appears to be broken. ERROR: openocd-stm32mp-native-0.11.0-rc2.AUTOINC+a5e526d857-r0 do_fe...
We are using OpenSTLinux as base distro for configuring and developing product on a custom STM32MP1 based embedded board. We plan to develop some testing and validation plans for the same. Just wanted to understand what sort of testing is carried out...
Hi all,I am trying to debug an C++ user space application on A7using STM32CubeIDE.Build happens fine. But when i try to debug it i run into following errors.I can confirm the toolchain is installed both on system as well as embedded in CUBEIDE.How ca...
Kudos from