User Activity

Hey there,I am trying to troubleshoot the following issue for quite some time now. I am working on an stm32mp157f based board attempting to enable a combination of stusb16xx and USB OTG . The behavior I am expecting to see is that when a usb device i...
Hi there, I am working on an OSD32MP157F custom board inspired by STM32MP157F-DK and Octavo Red boards. The pinout is very similar to the stm32mp157f-dk with the main difference that the Murata LBEE5kL1BX-883 is connected to sdmmc3 instead of sdmmc2 ...
Hi there, I am working on an STM32MP157F-DK2 board and an STUSB1600 with hsotg gadget support and no PD controller. I am running a buildroot image with all the necessary drivers enabled including dwc2, SystemFS etc.  The gadget is working as expected...
Hi there, I am working on a custom board based on OSD32MP157F. The pinout is very similar to the stm32mp157f-dk2 with the main difference that the Murata LBEE5kL1BX-883 is connected to sdmmc3 instead of sdmmc2 and that there is no ethernet peripheral...
Hey there, I am working with a custom board based on an OSD32MP157F SoM. The pinout is very similar with the DK2 board with some minor differences, mainly the DSI_RESET pin. I have done several tests on STM32MP157f-dk2 boards with an eDP display that...
Kudos from
Kudos given to