cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet Ping issue in UbootV2022.10

Srikanth1
Associate III

Hello,

We are using STM32157AAA3 Processor in our custom board and Microchip Ksz9893 switch for ethernet and the switch is configured using i2c.

  • when we are trying to ping ethernet in RGMII mode in U-Boot v2022.10-stm32mp-r1 we are getting the Rx-clock frequency 125MHz but the Tx clock is configuring for 2.5Mhz and we are getting ping is not alive.
  • when we try to ping ethernet in RMII Mode with auto negotiation it works fine.
  • And we are able to ping ethernet in linux(v5.13) with fixed-link property in rgmii and rmii but when we are trying to use fixed-link in ubootV2022.10 we are getting cpu reset issue.

Please find the below attached screen shots for our processor specific and board specific configurations and output log

  •     with out fixed-link we are getting without fixed-link propertywithout fixed-link property
  • with fixed-link we are getting

With fixed-link propertyWith fixed-link property

 

please help us in this regards.

regards,

Srikanth.

0 REPLIES 0