cancel
Showing results for 
Search instead for 
Did you mean: 

📡 Help Needed: STM32WB10CCU5 OTA Handler

SMazu.3
Associate III

Hi all,

I hope you're doing well. I'm working on a project with the STM32WB10CCU5 microcontroller and could use some help with setting up an OTA (Over-The-Air) update handler. I've searched through docs and examples but can't find a fit. Most resources are for similar models like STM32WB15 or STM32WB55.

If anyone has experience with the STM32WB10CCU5 or has implemented OTA updates on it, I'd appreciate any guidance or code snippets you could share.

Thanks for all,

0 REPLIES 0