cancel
Showing results for 
Search instead for 
Did you mean: 

I can't burn or debug a project on STM32 IDE

JRios
Associate II

I'm working with Windows 10 and STM Ide version 1.5.1.

I have a project made it with CubeMX.  I use FreeRTOS and some HAL libraries.

I can compile correctly:

arm-none-eabi-size  ST-2100.elf

arm-none-eabi-objdump -h -S ST-2100.elf > "ST-2100.list"

arm-none-eabi-objcopy -O binary ST-2100.elf "ST-2100.bin"

  text     data      bss      dec      hex   filename

 46372       20    16416    62808     f558   ST-2100.elf

Finished building: default.size.stdout

Finished building: ST-2100.bin

Finished building: ST-2100.list

I could debug it before, but now, when I try to debug it, I get same response:

STMicroelectronics ST-LINK GDB server. Version 5.7.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       Logging Level             : 1

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Disabled

       SWD Debug                 : Enabled

       InitWhile                 : Enabled

Waiting for debugger connection...

Debugger connected

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.6.0-RC3                 

     -------------------------------------------------------------------

ST-LINK SN : 066AFF485550755187253829

ST-LINK FW : V2J37M26

Board      : NUCLEO-L053R8

Voltage    : 3.25V

SWD freq   : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x442

Revision ID : Rev 1.0

Device name : STM32F09x/F030xC

Flash size : 256 KBytes

Device type : MCU

Device CPU : Cortex-M0

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a02004.srec

 File         : ST-LINK_GDB_server_a02004.srec

 Size         : 46396 Bytes

 Address      : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 22]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:02.267

Verifying ...

Error: Data mismatch found at address 0x08004064 (byte = 0x33 instead of 0x01)

Error: Download verification failed

Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.5.0.202011040924\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Debugger connection lost.

Shutting down...

STM32_Programmer_CLI.exe exists on that path, its version is 2.7.0-RC1

more stuff, appears a message window with this text:

 Error in final launch sequence:

 Failed to execute MI command:

 load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf

 Error message from debugger back end:

 Error finishing flash operation

 Failed to execute MI command:

 load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf

 Error message from debugger back end:

 Error finishing flash operation

 Failed to execute MI command:

 load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf

 Error message from debugger back end:

 Error finishing flash operation

 Error finishing flash operation

This error isn't new for me, last year some times I got this error, my solution was made a new workspace, import my project and then worked fine, but today I can't do it fix with my "recipe".

I create a new workspace, then a a new project from zero with CubeMX or ST Ide, generate code and then debug without a modification of generated code, I get always same response.

I updated ST Cube IDE from 1.5.1 to 1.6 and the problem persists.

I don't know what can I do to solve it.

Why appears a double slash on path?:

=> load C:\\ws-1.15\\ST-2100\\Debug\\ST-2100.elf

How I can resolve this?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
JRios
Associate II

Update:

I use a STM32F091RC microcontroller and a nucleo L053 or ST Link V2 for programming, behaviour is the same.

JOswa.1
Associate

This as a possible fix.

Today I tried programming the Nucleo G071RB with the X-NUCLEO_GFX01M1 LCD running the Demo program and got similar errors.

Since I usually buy my Dev board in pairs, the other G071RB worked first time.

These two boards are the same revision number, production date and even have serial numbers only 300 apart from each other.(Firmware version: V2J37M27)

Thanks for your answer. I'm so sorry, but I don't understand what is the solution.

Can you explain me with details, please?