cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H725 SMPS issue

BenUtzer
Associate

I am having and issue with a STM32H725RGV6.

After powering my board, I can see the SMPS output at 1.36V, which I have connected to the VCAP inputs.
I can also connect to the µC using the STM32CubeProgrammer.

However, after flashing a simple firmware, the SMSP output drops to 0V and I can not connect anymore. I am aware that this can be the result of an improper SMPS configuration (https://community.st.com/t5/stm32-mcus/unable-to-connect-to-stm32h7-devices/ta-p/49296). However, in my (cube generated) project am am calling

HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY)

so this should be correct. Additionally, I tried to upload a program with nothing but an infinite loop in main, and the problem still occurs.

When pulling BOOT0 high, the SMSP output becomes 1.36V again and I can connect again. This makes me believe, that everything is set-up correctly hardware-wise. Otherwise, the bootloader would not run. 

thank you for your help

STM32H725RGV6 power.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @BenUtzer and welcome to the community,

If you are using CubeMx to generate the code, I think you have the same issue as these threads:

Thread1

Thread2

Please confirm.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello @BenUtzer and welcome to the community,

If you are using CubeMx to generate the code, I think you have the same issue as these threads:

Thread1

Thread2

Please confirm.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
BenUtzer
Associate

Thank you very much. I can confirm that this was indeed the issue.

mƎALLEm
ST Employee

Issue fixed in CubeMx 6.14.0 (already available on ST website)

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.