Solved
FLASH.ld syntax error when upgrading to CubeMX v6.12.1
- September 19, 2024
- 45 replies
- 23591 views
Hello,
Since the latest release of CubeMX (6.12.1), I have been encountering syntax errors related to the "FLASH.ld" file. This issue only arises when I generate code while setting the Toolchain/IDE to CMake. I am using STM32H753IIKx. It seems that CubeMX does not specify which RAM to use when setting the Toolchain/IDE to CMake.
I have also included the FLASH.ld file that was generated for your reference.
Thanks for your help.