2024-11-27 02:08 AM
Hello,
I am encountering an issue while building a Yocto-based image for the STM32MP157F-DK2. The problem arises when attempting to fetch the gcnano-userland-multi-binary-stm32mp package. Below are the details of the issue:
Project Details
Yocto Version: Dunfell (OpenSTLinux 5.10-dunfell-mp1-23-11-01)
Target Machine: STM32MP157F-DK2
Recipe Name: gcnano-userland-multi-binary-stm32mp
Software Version: gcnano 6.4.3
Issue Description
The fetch operation fails due to a missing source file. Specifically:
However, this file is unavailable, and the fetch results in a 404 error.
Here is an excerpt from the build logs:
http://downloads.yoctoproject.org/mirror/sources/git2_github.com.STMicroelectronics.gcnano-binaries.tar.gz
Resolving downloads.yoctoproject.org (downloads.yoctoproject.org)... 2a01:4f9:3070:3985::2, 37.27.135.249
Connecting to downloads.yoctoproject.org (downloads.yoctoproject.org)|2a01:4f9:3070:3985::2|:80... connected.
HTTP request sent, awaiting response... 404 Not Found
2024-11-27 06:26:24 ERROR 404: Not Found.
Could you please provide updated instructions or a patch to resolve this fetch failure?