2025-01-20 9:55 AM
hi ST support team
I am designing a circuit using the STM32WB09KE chip.
However, when running the BLE_p2pServer example program from the package STM32Cube_FW_WB0_V1.1.0 and using the ST BLE Toolbox app (on iphone) to connect, I encounter a continuous disconnect issue.
I have changed the UART1 pins and am not using the LSE compared to the example code.
Could you help me resolve this problem?
2025-01-20 10:06 AM
So have you looked-up what reason 08 means?
Does it work on an ST board?
2025-01-20 5:40 PM
0x08 meaning connection timeout
I don't have an ST board, so I haven't been able to test the sample code on it. I'm not sure if my circuit design is causing any abnormalities
2025-01-21 12:16 AM
@tiennguyen wrote:I'm not sure if my circuit design is causing any abnormalities
Which is exactly the reason for trying it on an ST board!
Or, at least, some other known-good board.