Question
How stm32f429 disco uses ltdc if the mode isnt set correctly
Hi
I'm trying to understand something in the schematic the disco1 IM pins are set to 4-wire 8-bit serial I

In the picture below they are connected using the SB22-25 but I've checked the board and they are not soldered so it is not possible to set the manually

I cheked the ili9341 datasheet and you cant change the mode using register
But there a lot of examples that this baord using ltdc with the display with paralel rgb565 how is this possible if the mode is not set correctly