cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 Studio v6.0 - warning/issue "Type 'uint32_t' could not be resolved

RatheeshT
Associate II

I have installed SPC5 Studio version 6.0 on my Windows 10 PC and compiled sample code.

When compiling the project , i got below warning/issue "Type 'uint32_t' could not be resolved"

Q1: Can you give the solution for this?

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Rthan ,

it is a preprocessor configuration issue.

You should configure CDT in order to pick stdint.h.

it is located in c:\SPC5Studio-6.0\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.XXXXXXXXX\toolchain\

Best Regards

Erwan

View solution in original post

10 REPLIES 10

Need to include a file that defines the type or do so yourself.

​

Should be in stdint.h shouldn't it?

​

Check what include trees you pull in via config files, etc.

Check the Include Paths and ordering the compiler is using.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thankyou for the quick response, I am new to SPC5 studio, so i am not aware of this much.

Pls find the attached screenshot for analyzing/understanding the issue in detail.

Pls give your input about this issue

Erwan YVIN
ST Employee

Hello Rthan ,

it is a preprocessor configuration issue.

You should configure CDT in order to pick stdint.h.

it is located in c:\SPC5Studio-6.0\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.XXXXXXXXX\toolchain\

Best Regards

Erwan

Hi Erwan,

Thanks for your response.

I understands that it is preprocessor issue.

Can you guide me that what is CDT ? and how can i configure this on my project?

Hi Erwan,

The above screenshot shows the property screen of the project.

Is CDT equal to PATH in above screen? or Guide me the procedure to CDT configuration?

PChia.2237
Senior

Hi, i am newbee too, but i have solve 'uint32_t, 'uint16_t' 'uint8_t doing:

Right click on SPC5XXXXXTestApplication ->Properties

Under C/C++ General->Path and Symbols

Selec Tab Includes, then GNU C->Add..

write C:\SPC5Studio-6.0\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514\toolchain\include

I hope help somebody

VGani.1
Associate III

Hi PChia.2237

I have the include you mentioned, but I still have an error. "Type 'bool' could not be resolved". Asking for includes <stddef.h>,<stdbool.h>.

Looking for any suggestions. Thanks in advance.

PChia.2237
Senior

Yes, the something with this folder:

C:\SPC5Studio-6.0\eclipse\plugins\com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.20200908161514\toolchain\lib\gcc\powerpc-eabivle\4.9.4\include

You welcome. The problem is for SPC5 Studio 6. Version 5.8 has no this type of problem.

Really useful!!! TNX SO MUCH!!! you won the heven!!!