Solved
PROBLEM WITH X-NUCLEO-GNSS1A1 and NUCLEO-F446ZE
- 20 replies
- 12182 views
Hi I have connected the GNSS1A1 board and F446ZE boards. When I run the FW (Virtual Com Port) that I set up through STM32CUBE IDE (X-CUBE-GNSS) and start the program, when it enters MX_GNSS_Process() the gnssMsg struct's buffer pointer is pointing at reserved 0x2002 0000 address.

Then I tried generating the code for FW Updater example program, the Teseo Suit Can not do anything. It stops at Syncing, or if I try to force the update, at around 80% it freezes and recommends recovery mode. That doesn't work either.

Please help. I tried everything I2C or UART port but it looks like nothing is helping. The GetPos example is running fine, however gets no data.