Resolved! DEBUG ERROR
Hi, anyone know how to fix this debug error ?
Hi, anyone know how to fix this debug error ?
Hello,I wrote some codes and it worked succesfully. Then I wanted to add some global variable for computing a value but global variables which are added later, their values did not change, altough I set the refresh period setting ( while are changing...
Dear All,I work with SPC56EC64 and have a question about debugging. For debug, I use SPC5-UDESTK debugger. Now I can't access a flash. During programming popped communication error. Since I can't access the flash memory to read or write. If I configu...
Is it possible to disable JTAG completely on a SPC564B MCU using software?Reading the documentation about the censorship feature, it only seems to disable access to flash. Is it still possible to access SRAM and registers via JTAG when censorship is ...
Hello everyone,Is it possible to program the SPC570Sxx series microcontrollers (specifically, SPC570S40E1) in Linux? I have been using PLS UDE-STK for programming under Windows but as far as I know there is no Linux version of that. Debugging capabil...
I am asking because I created a second configuration (Now I have the " Default" and the "Release"). My goal is to find a way to force the linker to use one .ld file with the " Default" configuration and another .ld file with the "Release" configurat...
Posted on July 27, 2017 at 14:00Hi,I am using a SPC560C50L3 controller on a SPC560BADPT100S MINIMODULE board which sits on the XPC56XX EVB Motherboard. Power supply checked, jtag driver checked. The JTAG used is from PLS USB/JTAG Adapter for SPC5XXX...
Posted on April 17, 2015 at 10:55Hello,I am trying to execute a simple serial driver application on my target board. It uses SPC560D30L3 MCU. I have tested the same code using SPC Discovery kit (SPC560D30L3) mounted on it. The code executes successf...
Posted on July 09, 2007 at 09:24C Lib problem