Skip to main content
AMend.7
Associate III
November 22, 2022
Question

STM32N6

  • November 22, 2022
  • 13 replies
  • 12476 views

Hi,

When ST will release more information about the STM32N6? Will it use the new cortex-m55? Can it be used in motor control applications?

    This topic has been closed for replies.

    13 replies

    Miguel CASTRO
    ST Employee
    March 17, 2023

    Hi, getting close to that moment ;). We will share later this year more information about availability and spec and you will definitively be able to do motor control applications with it!

    Singh.Harjit
    Senior
    May 5, 2023

    @MC.4ASTRO​ any update on the date? I recently saw an ST press release.

    Miguel CASTRO
    ST Employee
    May 7, 2023

    Hi @Singh.Harjit​ , we are progressing well and so far no press release has been don eon the STM32N6 product. You will find information we are willing to share at this point on the following link https://blog.st.com/stm32n6/

    etheory
    Senior
    May 8, 2023

    Could we provide input in this process? I'd really like to make sure ST avoids the mistakes they made with the CORDIC and FMAC engines by making them too specific and not general enough (i.e. with CORDIC I could be able to reprogram it on the fly using DMA so I can autonomously use it for multiple tasks and for FMAC not being able to load the X1 and X2 values autonomously and sequentially mean that the opportunity to use it as a general purpose vector multiplier are lost. If you'd allowed those two things, you'd have had a beautiful hardware FFT capability which was missed). I'd just really like to make sure that the "ST Neural Processing Unit" can be used for more general vector/matrix operations on a LEAST signed 16bit data, preferably 32bit float, since this would mean that you can REALLY make use of it BOTH for NN/AI and ALSO for audio synthesis/processing/motor control etc. Please let us help you by providing feedback before it's too late and you've already committed missed opportunities to silicon.

    Miguel CASTRO
    ST Employee
    May 8, 2023

    Hi @etheory​, valuable feedbacks. Thanks for taking the time. I will pass to both Motor Control and AI teams.

    etheory
    Senior
    May 9, 2023

    How could I get more directly involved in this process? I have a lot of other feedback but this feels like the wrong forum for it.

    Miguel CASTRO
    ST Employee
    May 9, 2023

    Sure let me get back to you by private message.

    Associate II
    December 6, 2023

    Hello Miguel,

    Can I please be added to the list of people who will be notified when the STM32N6 development board is available?

    Thanks,

    Bruce

    Associate II
    February 9, 2024

    Hello @Miguel CASTRO ,

    Could I also please be added to the list of people who will be notified when the STM32N6 development board is available for purchase?

    Associate
    September 7, 2024

    Hello @Miguel CASTRO,

    It's been a while since the last update. Are there more details about the product and when it will be released? 

    Thank you, 

    Ramil

    DmitryR
    Associate III
    November 28, 2024

    Hi @ramil ,

     

    despite there is still no official announcement it is already available in the latest software updates (Cube and CubeIDE). Shortly:

    • M55 (with Helium I guess) at 800MHz
    • 4MB RAM, no internal flash
    • Rich in connectivity: 3xFDCAN, ETH, 2xSDMMC, 2xUSB OTG HS
    • Rich in multimedia (CSI, DCMI, GPU2D)
    • VFBGA only

     

    Regards,

    Dmitry

    Julian E.
    ST Technical Moderator
    November 28, 2024

    Hello everyone,

     

    I highly suggest you attend to the ST32 Summit on the 10th to the 13th of December and in particular, to register for the events on the 12th and 13th as they are dedicated to AI accelerated hardware and AI software solution

    STM32 Summit - STMicroelectronics

     

    Have a good day,

    Julian

    ​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.