2021-10-15 12:27 AM
Hi all, I got back on a project on the SPC574K2 I paused a few months ago and decided to start over from a green-field environment.
I then downloaded and installed SPC5Studio 6.0.0 Doyle which came along with version 1.16.1.20210914101245 of the LLD sdk.
Unfortunately my project builds fine but it is not running anymore due to a problem in board clock management (I', using the EVBoard)
To have proof of evidence for this I re-installed 6.0.0.Asimov (which instead comes with LLD version 1.13.1.20200626121018 with which, instead, my code (AND the EXAMPLES provided by ST) builds and runs just fine
Needless to say I'm pretty unhappy of this finding which came out without any explicit notice >:(
Has anyone run into similar issues? how did you got away?
Thanks in advance
Solved! Go to Solution.
2021-10-15 2:18 AM
Hello CoolMo,
Update on SPC574K2 RLA has been pushed in http://download.spc5studio.com/updates
You can update only the following feature
SPC5-RLA_SPC574Kxx_Support_Feature 1.16.2
Sorry for the issue ;)
Best Regards
Erwan
2021-10-15 1:09 AM
Hello CoolMo ,
We have well a clocking issue on K2 on Doyle
we are validating a patch and pushing a patch on SPC5RLA side asap.
http://download.spc5studio.com/updates
Best Regards
Erwan
2021-10-15 1:20 AM
Thank you very much for a prompt reply Erwan,
I'll keep an eye on the update release.
M
2021-10-15 2:18 AM
Hello CoolMo,
Update on SPC574K2 RLA has been pushed in http://download.spc5studio.com/updates
You can update only the following feature
SPC5-RLA_SPC574Kxx_Support_Feature 1.16.2
Sorry for the issue ;)
Best Regards
Erwan
2021-10-15 4:28 AM
Yes, I can confirm the examples now work with 1.16.2.
Thank you for prompt and quick acting.
one last thing: signing of plugin may need to be included for next releases (install anyway is possible and things work afterwards):
Thanks again
Mo
2021-10-15 5:36 AM
Hello CoolMo ,
We need to create a real signature in our next delivery workbench. (features & plugins)
you can click on "Install Anyway"
it is a change request in our process ;)
Best Regards
Erwan