2016-01-06 06:47 AM
Dear SPC5Studio Team,
I followed the installation procedure (backup licence and workspace, uninstall v3.7.1, remove workspace...) and I now have 2 problems: - I exported my v3.7 project in zip file and imported it in v4.0. I added the Platform, init and LL drivers SLA packages and I generate the components. WHERE COULD DRIVERS SETTINGS BE FOUND? The clock component shows clock settings, ok, but where are FlexCAN, DSPI settings??? Even if I create an app using the wizard, i'm stuck. The clock settings are not using the values I used in my configuation.xml. Is the v3.7 configuration.xml still supported in v4.0? - I set the http and https proxy settings to manual with correct server address, port, login and pwd, clear socks entries, and at startup the log says ''System property https.proxyPort is not set but should be 8080.'' and so on for all 6 properties. Only one time it worked after applying but when looking for updates or market place I had 2 possible issues: - 9 times out of 10, the log shows ''Provisioning exception'' containing ''HTTP Proxy Authentication Required: ''. OR - 1 time out of 10, the fetching starts but the transfer is extremely slow (2kB/s...) and stops after 20 minutes. The ST website is also very slow to respond. Is there any issues on the ST side or could this come from my proxy config? What would you recommand?2016-01-12 06:20 AM
Hello Aurelien ,
Could you confirm Hightec version ? Best Regards Erwan2016-01-13 01:30 AM
I'm using Hithtec Power PC toolchain v4.6.6.0.
To use a floating licence the key RLM_LICENSE has to be the port and server (e.g.mailto:5053@server
). I actually have the following problem: I couldn't solve this linker error: c:/hightec/toolchains/powerpc/v4.6.6.0/bin/../lib/gcc/ppc-ht-eabi/4.6.4/../../../../ppc-ht-eabi/bin/ld.exe: error: cannot find -lm ld.exe has no -lm option and I don't know where to correct this. I switched to the hightec/eclipse environment and it builds without any problem. Reagrds, Aurélien2016-01-13 07:50 AM
2016-01-14 08:28 AM
Hello Erwan,
see file attached. I added -lc option to linker settings without success. -lm was not set. Where should I correct this? Regards, Aurélien ________________ Attachments : 2016-01-14_172455.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qV8j&d=%2Fa%2F0X0000000bns%2FG_4djKyMxjD5ZjYzyiWPMd06LTwO4CbM9RbgG1Lehp4&asPdf=false2016-01-14 09:10 AM
Hello Aurelien ,
you should 1) unset your environment variable USE_LDOPT.in C/C++/Build/Environment 2) or Put this variable environment Empty Best regards Erwan2016-01-19 01:51 AM
Hello Erwan,
problem solved! I were right, I removed this key. Thank you