/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2021 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #define FLASH_STORAGE_M 0x08005000 #define FLASH_STORAGE_Q 0x08005500 #define page_size 0x800 /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void save_to_flash(uint8_t *data, uint32_t address) { volatile uint32_t data_to_FLASH[(strlen((char*)data)/4) + (int)((strlen((char*)data) % 4) != 0)]; memset((uint8_t*)data_to_FLASH, 0, strlen((char*)data_to_FLASH)); strcpy((char*)data_to_FLASH, (char*)data); volatile uint32_t data_length = (strlen((char*)data_to_FLASH) / 4) + (int)((strlen((char*)data_to_FLASH) % 4) != 0); volatile uint16_t pages = (strlen((char*)data)/page_size) + (int)((strlen((char*)data)%page_size) != 0); /* Unlock the Flash to enable the flash control register access *************/ HAL_FLASH_Unlock(); /* Allow Access to option bytes sector */ HAL_FLASH_OB_Unlock(); /* Fill EraseInit structure*/ FLASH_EraseInitTypeDef EraseInitStruct; EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.PageAddress = address; EraseInitStruct.NbPages = pages; uint32_t PageError; volatile uint32_t write_cnt=0, index=0; volatile HAL_StatusTypeDef status; status = HAL_FLASHEx_Erase(&EraseInitStruct, &PageError); while(index < data_length) { if (status == HAL_OK) { status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, address+write_cnt, data_to_FLASH[index]); if(status == HAL_OK) { write_cnt += 4; index++; } } } HAL_FLASH_OB_Lock(); HAL_FLASH_Lock(); } void read_flash(uint8_t* data,uint32_t address) { volatile uint32_t read_data; volatile uint32_t read_cnt=0; do { read_data = *(uint32_t*)(address + read_cnt); if(read_data != 0xFFFFFFFF) { data[read_cnt] = (uint8_t)read_data; data[read_cnt + 1] = (uint8_t)(read_data >> 8); data[read_cnt + 2] = (uint8_t)(read_data >> 16); data[read_cnt + 3] = (uint8_t)(read_data >> 24); read_cnt += 4; } }while(read_data != 0xFFFFFFFF); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); /* USER CODE BEGIN 2 */ /* USER CODE BEGIN 2 */ char write_data[50]; memset(write_data, 0, sizeof(write_data)); printf("going to write to flash"); strcpy(write_data, "Hello World!!!"); //save_to_flash((uint8_t*)write_data,FLASH_STORAGE_M); char read1_data[50]; memset(read1_data, 0, sizeof(read1_data)); read_flash((uint8_t*)read1_data,FLASH_STORAGE_M); int write_number = 23; int *pointer_write = &write_number; //save_to_flash((uint8_t*)pointer_write,FLASH_STORAGE_Q); int read2_number = 0; int *pointer_read = &read2_number; read_flash((uint8_t*)pointer_read,FLASH_STORAGE_Q); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13, GPIO_PIN_RESET); /*Configure GPIO pin : PC13 */ GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */