/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * *

© Copyright (c) 2021 STMicroelectronics. * All rights reserved.

* * This software component is licensed by ST under BSD 3-Clause license, * the "License"; You may not use this file except in compliance with the * License. You may obtain a copy of the License at: * opensource.org/licenses/BSD-3-Clause * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include // printf #include "visEffect.h" //#include "etaCom.h" #include "BSP_SGmini_MK2.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; DMA_HandleTypeDef hdma_adc1; SDADC_HandleTypeDef hsdadc1; DMA_HandleTypeDef hdma_sdadc1; TIM_HandleTypeDef htim2; TIM_HandleTypeDef htim5; TIM_HandleTypeDef htim15; TIM_HandleTypeDef htim19; UART_HandleTypeDef huart1; /* USER CODE BEGIN PV */ extern EncoderValues_t henc1; // encoder extern volatile int16_t brightness_bulbs; volatile uint16_t adc_dma_buffer [ SG_MK2_ADC1_CHANNELS * SG_MK2_ADC1_N_SAMPLES ]; volatile uint16_t sdadc_dma_buffer [ 3*16 ]; volatile uint8_t flag_ADC_cplt; volatile uint8_t flag_SDADC_cplt; float adc_voltages [ SG_MK2_ADC1_CHANNELS * SG_MK2_ADC1_N_SAMPLES ]; float adc_currents [ 3*16 ]; volatile uint8_t flag_PV_sufficientVoltage; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_TIM2_Init(void); static void MX_DMA_Init(void); static void MX_ADC1_Init(void); static void MX_USART1_UART_Init(void); static void MX_SDADC1_Init(void); static void MX_TIM15_Init(void); static void MX_TIM19_Init(void); static void MX_TIM5_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM2_Init(); MX_DMA_Init(); MX_ADC1_Init(); MX_USART1_UART_Init(); MX_SDADC1_Init(); MX_TIM15_Init(); MX_TIM19_Init(); MX_TIM5_Init(); /* USER CODE BEGIN 2 */ HAL_Delay(3000); HAL_GPIO_WritePin(USB_Enable_1_GPIO_Port, USB_Enable_1_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(USB_Enable_2_GPIO_Port, USB_Enable_2_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(ENABLE_DRIVE_BULB_GPIO_Port, ENABLE_DRIVE_BULB_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(ENABLE_DRIVE_DC_GPIO_Port, ENABLE_DRIVE_DC_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(ENABLE_IN_24VBUS_GPIO_Port, ENABLE_IN_24VBUS_Pin, GPIO_PIN_RESET); HAL_GPIO_WritePin(ENABLE_IN_SOLAR_GPIO_Port, ENABLE_IN_SOLAR_Pin, GPIO_PIN_SET); //HAL_ADCEx_Calibration_Start(&hadc1); // this should trigger DMA Half Transfer & DMA Transfer Complete Interrupts HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_dma_buffer, 4*16); __HAL_DMA_ENABLE_IT(&hdma_adc1, DMA_FLAG_HT1); __HAL_DMA_ENABLE_IT(&hdma_adc1, DMA_FLAG_TC1); //HAL_SDADC_InjectedStart_DMA(&hsdadc1, (uint32_t*)sdadc_dma_buffer, 3*16); //HAL_SDADC_InjectedMultiModeStart_DMA(&hsdadc1, (uint32_t*)sdadc_dma_buffer, 4*16); HAL_SDADC_InjectedStart_DMA(&hsdadc1, (uint32_t*)sdadc_dma_buffer, 3*16); __HAL_DMA_ENABLE_IT(&hdma_sdadc1, DMA_FLAG_HT1); __HAL_DMA_ENABLE_IT(&hdma_sdadc1, DMA_FLAG_TC1); /* HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1); // MPPT PWM HAL_TIMEx_PWMN_Start(&htim15, TIM_CHANNEL_1); // also start CH1N TIM15->CCR1 = 112;*/ HAL_TIM_Encoder_Start(&htim19, TIM_CHANNEL_1); HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1); // LED Bulb HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_2); // LED Bulb HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_3); // LED Bulb HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_4); // LED Bulb HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_1); // board LED HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_2); // board LED HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_3); // board LED HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_4); // board LED printf("SG Mini MKII\n"); uint8_t canAddress = BSP_Get_UserAddress(); printf("CAN Address: %d\n", canAddress); //etaCom_Init(canAddress+128); // I am a Remote Master with high priority address 32 //visInit(); // WS2812b Init (settings in ws2812b.h) /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ BSP_ReadSwitches(); // poll switches BSP_ReadEncoder(); // poll encoder BSP_SetUSBOutput(); // update USB switch state BSP_ChangeBulbBrightness(henc1.delta); // printf("%d --> %d\n", henc1.delta, brightness_bulbs); henc1.delta = 0; BSP_UpdateBulbBrightness(); for(uint8_t i=0; i<16; i++){ adc_currents[i*3+0] = BSP_conv_I_Boost(adc_dma_buffer[i*3+0]); adc_currents[i*3+1] = BSP_conv_I_MPPT (adc_dma_buffer[i*3+1]); adc_currents[i*3+2] = BSP_conv_I_Solar(adc_dma_buffer[i*3+2]); } //printf("DCDC\tMPPT\tPV\n"); //printf("%.3fA\t%.3fA\t%.3fA\n", adc_currents[0], adc_currents[1], adc_currents[2]); float temp = 0.0f; uint8_t index = 0; for(uint8_t i=0; i<8; i++){ temp = BSP_convU1(adc_dma_buffer[i*SG_MK2_ADC1_CHANNELS+0]); index = i*SG_MK2_ADC1_CHANNELS+0; adc_voltages[index] = temp; // BSP_convU1(adc_dma_buffer[i*SG_MK2_ADC1_CHANNELS+0]); adc_voltages[i*SG_MK2_ADC1_CHANNELS+1] = BSP_convU2(adc_dma_buffer[i*SG_MK2_ADC1_CHANNELS+1]); adc_voltages[i*SG_MK2_ADC1_CHANNELS+2] = BSP_convU3(adc_dma_buffer[i*SG_MK2_ADC1_CHANNELS+2]); adc_voltages[i*SG_MK2_ADC1_CHANNELS+3] = BSP_internalTemperature(adc_dma_buffer[i*SG_MK2_ADC1_CHANNELS+3]); } //printf("\nPV\tCAN\tBat\tTemp\n"); //printf("%.2fV\t%.2fV\t%.2fV\t%.1fC\n", adc_voltages[0], adc_voltages[1], adc_voltages[2], adc_voltages[3]); float pwr = BSP_averagePower( &adc_voltages[0], &adc_currents[2], SG_MK2_ADC1_CHANNELS, SG_MK2_SDADC1_CHANNELS, 1); //printf("%.5fV * %.5fA = %.5fW\n", adc_voltages[0], adc_currents[2], pwr); printf("\n%d\t%d\t%d\t%d\n", adc_dma_buffer[0], adc_dma_buffer[1], adc_dma_buffer[2], adc_dma_buffer[3]); printf("%.2f\t%.2f\t%.2f\t%.2f\n", adc_voltages[0], adc_voltages[1], adc_voltages[2], adc_voltages[3]); printf("%.2f\t%.2f\t%.2f\n", BSP_convU1(adc_dma_buffer[0]), BSP_convU2(adc_dma_buffer[1]), BSP_convU3(adc_dma_buffer[2])); HAL_Delay(100); // visHandle(); } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_PeriphCLKInitTypeDef PeriphClkInit = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_ADC1 |RCC_PERIPHCLK_SDADC; PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2; PeriphClkInit.SdadcClockSelection = RCC_SDADCSYSCLK_DIV16; PeriphClkInit.Adc1ClockSelection = RCC_ADC1PCLK2_DIV2; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); } HAL_PWREx_EnableSDADC(PWR_SDADC_ANALOG1); } /** * @brief ADC1 Initialization Function * @param None * @retval None */ static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Common config */ hadc1.Instance = ADC1; hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 4; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_6; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_71CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_7; sConfig.Rank = ADC_REGULAR_RANK_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_REGULAR_RANK_3; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_TEMPSENSOR; sConfig.Rank = ADC_REGULAR_RANK_4; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ } /** * @brief SDADC1 Initialization Function * @param None * @retval None */ static void MX_SDADC1_Init(void) { /* USER CODE BEGIN SDADC1_Init 0 */ /* USER CODE END SDADC1_Init 0 */ SDADC_ConfParamTypeDef ConfParamStruct = {0}; /* USER CODE BEGIN SDADC1_Init 1 */ /* USER CODE END SDADC1_Init 1 */ /** Configure the SDADC low power mode, fast conversion mode, slow clock mode and SDADC1 reference voltage */ hsdadc1.Instance = SDADC1; hsdadc1.Init.IdleLowPowerMode = SDADC_LOWPOWER_NONE; hsdadc1.Init.FastConversionMode = SDADC_FAST_CONV_DISABLE; hsdadc1.Init.SlowClockMode = SDADC_SLOW_CLOCK_DISABLE; hsdadc1.Init.ReferenceVoltage = SDADC_VREF_EXT; hsdadc1.InjectedTrigger = SDADC_SOFTWARE_TRIGGER; if (HAL_SDADC_Init(&hsdadc1) != HAL_OK) { Error_Handler(); } /** Configure the Injected Mode */ if (HAL_SDADC_SelectInjectedDelay(&hsdadc1, SDADC_INJECTED_DELAY_NONE) != HAL_OK) { Error_Handler(); } if (HAL_SDADC_SelectInjectedTrigger(&hsdadc1, SDADC_SOFTWARE_TRIGGER) != HAL_OK) { Error_Handler(); } if (HAL_SDADC_InjectedConfigChannel(&hsdadc1, SDADC_CHANNEL_4|SDADC_CHANNEL_8 |SDADC_CHANNEL_6, SDADC_CONTINUOUS_CONV_ON) != HAL_OK) { Error_Handler(); } /** Set parameters for SDADC configuration 0 Register */ ConfParamStruct.InputMode = SDADC_INPUT_MODE_SE_OFFSET; ConfParamStruct.Gain = SDADC_GAIN_1; ConfParamStruct.CommonMode = SDADC_COMMON_MODE_VSSA; ConfParamStruct.Offset = 0; if (HAL_SDADC_PrepareChannelConfig(&hsdadc1, SDADC_CONF_INDEX_0, &ConfParamStruct) != HAL_OK) { Error_Handler(); } /** Configure the Regular Channel */ if (HAL_SDADC_AssociateChannelConfig(&hsdadc1, SDADC_CHANNEL_6, SDADC_CONF_INDEX_0) != HAL_OK) { Error_Handler(); } /** Configure the Injected Channel */ if (HAL_SDADC_AssociateChannelConfig(&hsdadc1, SDADC_CHANNEL_4, SDADC_CONF_INDEX_0) != HAL_OK) { Error_Handler(); } /** Configure the Injected Channel */ if (HAL_SDADC_AssociateChannelConfig(&hsdadc1, SDADC_CHANNEL_8, SDADC_CONF_INDEX_0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN SDADC1_Init 2 */ /* USER CODE END SDADC1_Init 2 */ } /** * @brief TIM2 Initialization Function * @param None * @retval None */ static void MX_TIM2_Init(void) { /* USER CODE BEGIN TIM2_Init 0 */ /* USER CODE END TIM2_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM2_Init 1 */ /* USER CODE END TIM2_Init 1 */ htim2.Instance = TIM2; htim2.Init.Prescaler = 280; htim2.Init.CounterMode = TIM_COUNTERMODE_UP; htim2.Init.Period = 256-1; htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim2) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim2) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_4) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM2_Init 2 */ /* USER CODE END TIM2_Init 2 */ HAL_TIM_MspPostInit(&htim2); } /** * @brief TIM5 Initialization Function * @param None * @retval None */ static void MX_TIM5_Init(void) { /* USER CODE BEGIN TIM5_Init 0 */ /* USER CODE END TIM5_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM5_Init 1 */ /* USER CODE END TIM5_Init 1 */ htim5.Instance = TIM5; htim5.Init.Prescaler = 280; htim5.Init.CounterMode = TIM_COUNTERMODE_UP; htim5.Init.Period = 256-1; htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim5.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim5) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim5, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim5) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim5, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim5, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim5, &sConfigOC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim5, &sConfigOC, TIM_CHANNEL_3) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim5, &sConfigOC, TIM_CHANNEL_4) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM5_Init 2 */ /* USER CODE END TIM5_Init 2 */ HAL_TIM_MspPostInit(&htim5); } /** * @brief TIM15 Initialization Function * @param None * @retval None */ static void MX_TIM15_Init(void) { /* USER CODE BEGIN TIM15_Init 0 */ /* USER CODE END TIM15_Init 0 */ TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0}; /* USER CODE BEGIN TIM15_Init 1 */ /* USER CODE END TIM15_Init 1 */ htim15.Instance = TIM15; htim15.Init.Prescaler = 5; htim15.Init.CounterMode = TIM_COUNTERMODE_UP; htim15.Init.Period = 120-1; htim15.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim15.Init.RepetitionCounter = 0; htim15.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_PWM_Init(&htim15) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim15, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET; sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET; if (HAL_TIM_PWM_ConfigChannel(&htim15, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE; sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE; sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF; sBreakDeadTimeConfig.DeadTime = 0; sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE; sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH; sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE; if (HAL_TIMEx_ConfigBreakDeadTime(&htim15, &sBreakDeadTimeConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM15_Init 2 */ /* USER CODE END TIM15_Init 2 */ HAL_TIM_MspPostInit(&htim15); } /** * @brief TIM19 Initialization Function * @param None * @retval None */ static void MX_TIM19_Init(void) { /* USER CODE BEGIN TIM19_Init 0 */ /* USER CODE END TIM19_Init 0 */ TIM_Encoder_InitTypeDef sConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM19_Init 1 */ /* USER CODE END TIM19_Init 1 */ htim19.Instance = TIM19; htim19.Init.Prescaler = 0; htim19.Init.CounterMode = TIM_COUNTERMODE_UP; htim19.Init.Period = 65535; htim19.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim19.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; sConfig.EncoderMode = TIM_ENCODERMODE_TI1; sConfig.IC1Polarity = TIM_ICPOLARITY_RISING; sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI; sConfig.IC1Prescaler = TIM_ICPSC_DIV1; sConfig.IC1Filter = 0; sConfig.IC2Polarity = TIM_ICPOLARITY_RISING; sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI; sConfig.IC2Prescaler = TIM_ICPSC_DIV1; sConfig.IC2Filter = 0; if (HAL_TIM_Encoder_Init(&htim19, &sConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim19, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM19_Init 2 */ /* USER CODE END TIM19_Init 2 */ } /** * @brief USART1 Initialization Function * @param None * @retval None */ static void MX_USART1_UART_Init(void) { /* USER CODE BEGIN USART1_Init 0 */ /* USER CODE END USART1_Init 0 */ /* USER CODE BEGIN USART1_Init 1 */ /* USER CODE END USART1_Init 1 */ huart1.Instance = USART1; huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART1_Init 2 */ /* USER CODE END USART1_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); __HAL_RCC_DMA2_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Channel1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn); /* DMA2_Channel3_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA2_Channel3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA2_Channel3_IRQn); } /** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOF_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOE_CLK_ENABLE(); __HAL_RCC_GPIOD_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, ENABLE_DRIVE_DC_Pin|ENABLE_DRIVE_BULB_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(ENABLE_IN_SOLAR_GPIO_Port, ENABLE_IN_SOLAR_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(ENABLE_IN_24VBUS_GPIO_Port, ENABLE_IN_24VBUS_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_Enable_1_GPIO_Port, USB_Enable_1_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(USB_Enable_2_GPIO_Port, USB_Enable_2_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : SW_USB_1_Pin SW_ENC_Pin Adr_2_Pin Adr_3_Pin Adr_1_Pin */ GPIO_InitStruct.Pin = SW_USB_1_Pin|SW_ENC_Pin|Adr_2_Pin|Adr_3_Pin |Adr_1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*Configure GPIO pins : ENABLE_DRIVE_DC_Pin ENABLE_DRIVE_BULB_Pin */ GPIO_InitStruct.Pin = ENABLE_DRIVE_DC_Pin|ENABLE_DRIVE_BULB_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : ENABLE_IN_SOLAR_Pin */ GPIO_InitStruct.Pin = ENABLE_IN_SOLAR_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(ENABLE_IN_SOLAR_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : ENABLE_IN_24VBUS_Pin */ GPIO_InitStruct.Pin = ENABLE_IN_24VBUS_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(ENABLE_IN_24VBUS_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : USB_Enable_1_Pin */ GPIO_InitStruct.Pin = USB_Enable_1_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_Enable_1_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : USB_Enable_2_Pin */ GPIO_InitStruct.Pin = USB_Enable_2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(USB_Enable_2_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : SW_add_Pin */ GPIO_InitStruct.Pin = SW_add_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(SW_add_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : Adr_4_Pin */ GPIO_InitStruct.Pin = Adr_4_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(Adr_4_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : SW_Bulb_4_Pin SW_Bulb_1_Pin SW_Bulb_3_Pin SW_Bulb_2_Pin */ GPIO_InitStruct.Pin = SW_Bulb_4_Pin|SW_Bulb_1_Pin|SW_Bulb_3_Pin|SW_Bulb_2_Pin; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); } /* USER CODE BEGIN 4 */ /** * @brief Retargets the C library printf function to the USART. * @param None * @retval None */ PUTCHAR_PROTOTYPE { /* Place your implementation of fputc here */ /* e.g. write a character to the EVAL_COM1 and Loop until the end of transmission */ HAL_UART_Transmit(&huart1, (uint8_t *) &ch, 1, 0xFFFF); return ch; } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */ /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/